This ZIP File is associated with Rev 2 of the Application Note


    Cycle Counting and Profiling (EE-332)  


that can be found at http://www.analog.com/ee-notes.


Date Created:	March 27th, 2008



*****************************************************************************************


The archive provides 6 projects in total.

For a Profiling demonstration there are 3 projects and one source file:

	"21369-EZ-KIT Lite.dpj" in the directory ".\Profiling\21369-EZ-KIT Lite" is the project file
	for use with the SHARC 21369 EZ-KIT Lite.

	"BF533-EZ-KIT Lite.dpj" in the directory ".\Profiling\BF533-EZ-KIT Lite" is the project file
	for use with the Blackfin BF533 EZ-KIT Lite.

	"TS201-EZ-KIT Lite.dpj" in the directory ".\Profiling\TS201-EZ-KIT Lite" is the project file
	for use with the TigerSHARC TS201 EZ-KIT Lite.

	"main.c" is the source file used by the above projects to demonstrate the 
	profiling tools, as per Appendix A of the EE-Note.


For a Cycle Counting demonstration there are 3 projects and one source file:

	"21369-EZ-KIT Lite.dpj" in the directory ".\Cycle Counting\21369-EZ-KIT Lite" is the project file
	for use with the SHARC 21369 EZ-KIT Lite.

	"BF533-EZ-KIT Lite.dpj" in the directory ".\Cycle Counting\BF533-EZ-KIT Lite" is the project file
	for use with the Blackfin BF533 EZ-KIT Lite.

	"TS201-EZ-KIT Lite.dpj" in the directory ".\Cycle Counting\TS201-EZ-KIT Lite" is the project file
	for use with the TigerSHARC TS201 EZ-KIT Lite.

	"main.c" is the source file used by the above projects to demonstrate the 
	Cycle Counting Macros, as per Appendix B of the EE-Note.



*****************************************************************************************


All code examples have been written and tested with

	VisualDSP++ 5.0 Update 2

	ADSP-21369 revision 0.2
	ADSP-21369 EZ-KIT Lite revision 2.1

	ADSP-BF533 revision 0.5
	ADSP-BF533 EZ-KIT Lite revision 2.1

	ADSP-TS201 revision 2.0
	ADSP-TS201 EZ-KIT Lite revision 2.1


*****************************************************************************************